Tool/software:
Hello E2E Experts,
Good day.
mmWave Vital Signs Lab | Video | TI.com
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello E2E Experts,
Good day.
mmWave Vital Signs Lab | Video | TI.com
Hi,
We are looking into your query. Please allow us a couple of days to respond
Regards,
Sharan
Hi,
1. The demo provides an accuracy of +/-10 BPM for heart rate and +/-5 for breath rate. There are occasional jumps that happen which needs to be corrected. But generally heart rate is correct when the breathing rate is stable
2.Accuracy primarily depends on the movement of the person. If the person is stationary for more than 20 seconds, it is possible to achieve the accuracy as specified above
3.Yes, you can improve the accuracy based on improvement in the algorithm The current algorithm is based on the publicly available papers. More filtering can be added to reduce the jumps in measurements
4. The current demo can measure in the range of 60-110 BPM. The maximum heart rate is limited by the chirping scheme chosen for the demo. It is possible to increase the max rate
Regards