Other Parts Discussed in Thread: MMWAVE-L-SDK
Tool/software:
While playing with the "UART Echo Callback" example, I found out that `UART_write()` does not generate a callback if `UART_Transaction.count = 1`. So, I cannot implement this example to receive 1 character and echo back the same. Everything works fine except that I do not see the activation of `uart_echo_write_callback()`. I tested it for MMWAVE-L-SDK 05.04.00.01 and 05.05.02.00 and both results were negative. Does this mean that I cannot use all the features of `UART_write()` in interrupt mode if I have a reason to transmit only 1 character?
Thanks,
Alex.