This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: syncing beam calibration of multiple radars

Part Number: IWR6843AOPEVM

Tool/software:

I have multiple eval boards and I would like to edit their calibration parameters so they can behave similarly if possible. Any suggestions?

Are these radars calibrated? How can I access the calibration look up table if any?

Some eval boards give slightly higher power than others, is there a way to manipulate that internally?

  • Hi,

    We are looking into your query. Please allow us a couple of days to respond.

    Regards,

    Sharan

  • Hi

    It is not recommended to change the calibration data of individual devices. Calibration data makes sure that all devices behave as per the specification.

    Calibration data is stored in flash. All devices will behave differently without the calibration, also, calibration data is device specific, if the calibration data is interchanged then the device behaviour will be affected and it is not possible to achieve the correct performance. It is recommended that calibration data is not alter with

    Regards