This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: Detecting surface shape with radar IWR1443

Part Number: IWR1443


Tool/software:

Dear Ti experts.

I have the following requirement and would like to ask you a few questions.

For some coal bunkers or silos, I want to measure the shape of the surface of the material.
For example, as shown in the figure below.

Can I use a single chip (such as IWR1443, or other IWR series) to measure the surface shape of the material?

If so, how many Tx and Rx are needed to complete it?

If so, can you introduce the main algorithm and calculation ideas?

Does Ti have relevant examples for reference?

——
Or, if it cannot be completed with a single chip, what is the reason? Do we need cascade chips to complete it? Can you introduce the solution?