Tool/software:
hello.
I've been learning about radar recently, and I'm sorry for the lack of knowledge.
I am currently using the IWR1843BOOST radar sensor to collect IF signals at each distance from a fixed material (e.g. marble, tile, wood, etc.) and create an algorithm to classify the signals accordingly to identify the material.
During the signal acquisition process, do I need to worry about interference and overlapping scattering due to multiple paths on the floor or walls?
When I read the papers that use the radar provided by TI, I felt like I was experimenting without worrying about the above.
1. if you don't have to care, why?
2. if I do care, do I need to vary the surroundings or pay attention to signal pre-processing and filtering?
3. and I know that radar spreads radially and the FOV is -60° to +60°. Is the signal that is mainly collected is the signal reflected from the front relative to the antenna?
4. when collecting signals based on distance, is it almost the same to collect 20 times with a frame of 20 or 20 times with a frame of 1?
Please note that I don't have a finalised experimental setup yet, and I will send you some random experimental pictures and radar parameters. (Consider detailed experimental setup later)
Thank you for your insights!


Radar Parameter
- Number of Transmitters (Tx): 1
- Number of Receivers (Rx): 4
- Frequency Slope: 30.030 MHz/μs
- Ramp End Time: 130 μs
- ADC Samples per Chirp: 256
- Number of Chirps per Frame: 128
- Number of Frames: 20