Tool/software:
Hi team,
Do we have this kind of temperature switch support remote NTC?
Thanks!
Jayden Li
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jayden,
If the question is wether the device can use an NTC to trigger the switch output then the answer is no. This kind of switch device uses an external resistor to trigger at a set temperature compared to the internal temperature sensor of the device itself (TMP708). Not a remote junction or temperature sensing element.
Most NTC switches are implemented using a comparator circuit. If the question is whether we could replace an NTC + comparator solution then the answer is yes. The NTC + comparator would be replaced by the TMP708 device alone.
Best regards,
Simon Rojas