Tool/software:
I am using LM91000EVM board and using O2 lead-free sensor which has -600mV bias and 100uA output at ambient air. Issue is that my bias is not being set and even after keeping it for an 2-3 Hour it does not respond. I am supplying 3.0V to LMP91000. Below is my settings.
TIA GAIN = 350k Ohm,
RLOAD = 33 Ohm,
Vref = internal source,
Vref divider = 20%,
Bias sign = Negative
is there any other issue with the settings?
Thank you so much in advance