This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Enhancing IWR6843ISK with DCA1000EVM and MMWAVEICBOOST

Part Number: DCA1000EVM
Other Parts Discussed in Thread: IWR6843ISK, MMWAVEICBOOST

Tool/software:

I recently purchased the IWR6843ISK sensor and plan to enhance its performance by integrating it with the DCA1000EVM for raw data capture and algorithm refinement.
I would like to confirm whether the operating frequency of the IWR6843ISK can be adjusted beyond its default frequency range (60-70 GHz) when using the DCA1000EVM. If frequency customization is possible, could you please provide the necessary steps or guidelines to achieve this.
Do the IWR6843ISK, DCA1000EVM, and MMWAVEICBOOST require firmware updates to function optimally together? Are there guides or examples for tuning detection parameters (e.g., range, sensitivity) to suit specific project needs? and also what are the exact power specifications and requirements for these devices during standalone and integrated operation?
595-IWR6843ISK
595-DCA1000EVM
595-MMWAVEICBOOST