This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMCS1101: Output for TMCS1101A3U is 100mV/A instead of 200mV/A

Part Number: TMCS1101


Tool/software:

Hello,

We have bought a bunch of TMCS1101A3U only to find that the output scales at 100mV/A instead of 200mV/A (from the datasheet). This is frankly unacceptable, I see that TI has seen this issue before and it was supposed to be resolved. Why are we still seeing the same issue 3 years later? We have confirmed that the code on the IC matches properly, so it is indeed marked as a TMCS1101A3U.

Could someone please reach out to me to provide me a link to parts which actually work as detailed in the spec sheet?

Thanks,

Nikhil