Tool/software:
Hello,
I have some questions and requests about Antenna characteristics data of IWR1843AOP.
I would like to get either data 1) or 2) of IWR1843AOP for technical standards compliance (Japan).
1) Antenna gain data of the three transmitters (79GHz)
These antenna gain data requires the radiation pattern of Azimuth and Elevation planes, and it must be the maximum value.
Also it requires the data for three transmitter antennas(TX1, TX2, TX3).
Could you please send me these antenna gain data of the three transmitters of IWR1843AOP?
If you don't have these data, could you please measure them?
2) EIRP data of the three transmitters and Chip output power (79GHz)
These data requires the maximum value data and the data for three transmitter antennas(TX1, TX2, TX3).
There are the graph of EIRP radiation patterns of Azimuth and Elevation planes for Transmitter in the datasheet Page39,
but they are average EIRP data. I need maximum EIRP data.
I understand Chip output power is about 12dBm from following thread, but I would like to know maximum Chip output power of 79GHz.
It you don't have these data, could you please measure them?
Please advise.
Regards,
Shoko
Shoko-san,
In regards to #1, the antenna gain of the IWRL1843AOP is impossible to measure separately from the total device EIRP. This is intrinsic to the fact that the antennas are inegrated into the package.
For case #2, please contact your local TI representatives as this data cannot be released through a forums request.
Thanks,
Blake
Hello Blake,
Thanks for reply.
Please let me know contact address of local TI representative on direct message.
Regards,
Shoko