This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: IWR6843AOP

Part Number: IWR6843AOP

Tool/software:

Hi Sir,

I would like to ask the chirp_configs from 3D_People_Tracking (AOP_9m_default, AOP_6m_default)

AOP_9m_default.cfg:    profileCfg 0 60.75 30.00 25.00 59.10 394758 0 36 1 96 2950.00 2 1 36 

AOP_6m_default.cfg:    profileCfg 0 60.75 30.00 25.00 59.10 394758 0 54.71 1 96 2950.00 2 1 36

If I would like to use these two config (BW>1GHz) will these two config will pass the FCC short range critera? peak conductive: -10dBm

(TI default conducted is equal 12dBm, if need to pass FCC short range conductive requirement that means the RF power need to tx backoff to 22dB, right?

Can you provide the IWR6843AOP profile that can meet FCC requirement with higher BW with or more 2GHz for good range resolution, and the maximum distance detection for FOV120(+/-60) can cover 8m, boresight detection can cover 10m

thanks.