This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMAG5273-MSPM0L1306-CODE-EXAMPLE: TMAG3001evm

Part Number: TMAG5273-MSPM0L1306-CODE-EXAMPLE
Other Parts Discussed in Thread: TMAG3001EVM, MSPM0L1306, TMAG3001, CCSTUDIO, SYSCONFIG

Tool/software:

I am successfully running TI project TMAG3001evm_LP=mspm0l_updated from Alison of TI, similar to TMAG 5273, and separately successfully running  Project uart_tx_console_multibyte_repeated_fifo_dma_LP_MSPM0L1306_nortos_ticlang from mspm0Lexamples.The TMAG 3001 uses I2C, and the  1306 uses a UART

What I need to do is retrieve an angle calculation from the TMAG3001 and send it by UART to my PC via an external Uart to USB adapter. I cannot do this using the typical debug serial connection. I am using mspm0L1306 MPU 

I am having no luck in trying to integrate the two projects.. I've wiped out old CCStudio and CCStudioTheia several times and had to reinstall them. Can you provide some direction in how to proceed.?

I looked on the internet and find that the suggested way to proceed is create an empty file and start adding code.

Almost all the code in both files is automatically generated by Sysconfig. One thought is to start with a SysConfig from 1 project, and modify SysConfig by adding in the second project differences on the graphic SysConfig display. Will this work?

Is their a different approach?

I think TI should add an example or two which illustrates both I2C and uart .in the same project.

eric@avidasw.com  edulicki@avidasw.com

  • So you need an example about UART to I2C master bridge?

    In fact I think your approach is good(start with a SysConfig from 1 project, and modify SysConfig by adding in the second project differences on the graphic SysConfig display). To debug the function, you can disable one part and test another part. If both parts work well, then you can test them together.

  • Normal editing by adding code to a syscfg file in MAG was not allowed by TI. When I began to try to modify the graphic SysConfig for the TMAG 3001 I accidentally eliminated 1 GPIO. This subsequently caused CCStudioTheia build to fail. I had to delete the project then import it again to get back to ground zero.

  • What is the status now? Can you run the code well now?

  • At first I couldn't get revised Sysfig to change files. Then I deleted all 8 files under Debug>syscfg and rebuilt. That seemed to correct everything. Now I can modify .syscfg, save it, then rebuild. This works.