Tool/software:
Hi.
When the antenna was connected to IWR6843 and operated, the EIRP decreased as the antenna temperature increased.
(Tx1:40°C→EIRP:13.5dBm, Tx1:60°C→12.7dBm)
Antenna temperatures were obtained from IWR6843.
Calibration is performed at startup, but not on a regular basis.
Is this change in EIRP with temperature due to a change in the current supplied from IWR6843 to the antenna?
Does the supply current of IWR6843 vary with junction temperature?
If so, please provide documentation showing the relationship between temperature and supply current.
Thank you.