This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: High reflectance saturation phenomenon

Part Number: OPT3101


Tool/software:

In the process of using opt3101, no matter how small the current is used, such as 1.4mA. When encountering objects with high reflectivity (aluminum or stainless steel), there will be a phenomenon of saturation, and the amplitude output is 65535. What can be done to reduce this phenomenon?