This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: Is it possible to generate multiple Fls configurations in Tresos

Part Number: AWR2944

Tool/software:

Hi, 

In EB Tresos, is it possible to generate multiple Fls configurations, so we can choose which configuration to use on runtime.

I can see that we can add multiple devices to the FlsFlashConfigList.

Only one configuration is generated based on FlsExternalFlashSelect, where we select only one of the config from the list.

I'm looking for a way to generate multiple configurations and be selectable during run-time.

Is it possible with current package? If yes, any input on how is appreciated.

Thanks.