Other Parts Discussed in Thread: IWRL6432AOP
Tool/software:
Hi TI team,
I have questions about the power consumption of radar sensor. (IWR6843AOP and IWRL6432AOP)
[1] When we say the power consumption of radar sensor, which definition and numbers are we using generally?
There are lots of numbers and descriptions related power consumption. What is the reasonable to use?
For example, max power during active state, average power between active on and active off, etc.
[2] Based on the answer above, what are the power consumption of IWR6843AOP and IWRL6432AOP?
I can find several numbers in the datasheet but little bit confused which number should I use in general.
I would appreciate it if you answer my questions.
Thanks