This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1614EVM:   LDC1614EVM:antenna with frequency splitting

Part Number: LDC1614EVM


Tool/software:

Hello,

I would like to ask if we lock an antenna with frequency splitting within 10MHz (5.6Mz and 9.6MHz) to the CH0 channel, which value will the LDC1614EVM choose as the resonant frequency? Why was this value chosen? What are the selection criteria and basis? Where is this basis mentioned in the datasheet?


I look forward to your reply to help me clear up my doubts, thank you!

  • Lyu,

    I am not aware of an analysis or model that will predict the behavior of the system you have described.

    You will probably have to build the system and measure its behavior.

    regards,
    John

  • Hi,

    I have build the system and measure its behavior.

    If we lock an antenna with frequency splitting within 10MHz (5.6MHz and 9.6MHz) to the CH0 channel, 5.6MHzwill the LDC1614EVM choose as the resonant frequency.Where is this basis mentioned in the datasheet?

    Best regards,

    Lyu

  • Lyu,

    Our data sheet only considers a single dominant resonant circuit on the sensor.
    My guess is that it will tend to oscillate at the frequency whose corresponding circuit has the lowest equivalent parallel resistance, Rp.
    If all other parameters (equivalent L, C) are the same when comparing the two frequencies, then it will tend to correspond to the lowest frequency.

    Regards,
    John