Other Parts Discussed in Thread: IWR6843, UNIFLASH
Tool/software:
Hello,
I have some query related to RADAR module IWR6843AOP
1. I have read that we can IWR6843 module has Temperature IC on it, so we want to extract temperature value that present on RADAR IC, how we can extract that temperature.
2. We want to do some test on IWR6843 AOP module that required and suggested by TI for RADAR module this test are given below, How we can perform this test. Now we are using demo Application "3D People tracker" using this Application how we can do this activity?
| T4-1 | SOP[2.1.0] 101 (FLASH mode), Connect to the Control UART with Uniflash, or using CCS custom - program the Mss/Dss image + BSS patch | QSPI Flash update test OK |
| T4-2 | SOP[2.1.0] 001 (Functional mode), if using Out of Box demo, connect Control UART to terminal emulator, on nRESET release, software loads, type "ver" enter, should display the software version. | check QSPI Flash ->RAM, startup operation |
| T4-3 | Using driver test code in the SDK perform GPIO write read tests | GPIO function on customer board |
| T4-4 | Using driver test code in the SDK perform SPI read/write checks. This can be done for both secondary and primary modes. | SPI functions on customer board |
| T4-5 | Using driver test code in the SDK perform UART read/write checks. | UART functions on customer board |
| T4-6 | Using driver test code in the SDK perform CAN transmit/receive checks. | CAN functions for xWR6843AOP on customer board |
| T4-7 | Using driver test code in the SDK perform I2C read/write checks. | I2C functions on customer board |