This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-DSP-EVM: Is There a Device-Specific Identifier for the EVM

Part Number: MMWCAS-DSP-EVM
Other Parts Discussed in Thread: AWR2243, MMWCAS-RF-EVM,

Tool/software:

Hi, Experts!

[cascade_radar_object_detect] usecase of PROCESSOR_SDK_RADAR_03_08_00_00 is being used, AWR2243 MMWCAS-RF-EVM and companion MMWCAS-DSP-EVM are used.

I’m currently working with multiple development boards, and I need to control and differentiate them. I’m wondering if there is a unique device-specific identifier, like a device ID, that can be used to bind to each device.

If such an identifier exists, could you please point me to the relevant code or location where it is defined? Additionally, is it possible to modify or set this device ID ?

Thank you in advance! 

Liam