Tool/software:
I have some questions about the AWR2944 radar sensor. I would like to adapt it for human rescue application.
1. Is it possible to configure the radar sensor frequency range from 76-81GHz to 300Mhz-3GHz ? In this range, radar waves have better penetration under ground. We would like to adapt your sensor for USAR (Urban search & Rescue) application
2. In which format can we get the data output out of your sensor ? Raw ADC data ? UDP packets (till you are speacking about an Ethernet output interface) ?
3. Is there any first stage filtering done inside the radar sensor ?
4. Is the some human recognition algorithm done inside the radar sensor ?
5. It is possible to connect the radar sensor to 8 Tx and 8 Rx antennas. Could you please tell us if it is the only combination possible ? E.g 2 Tx and 6 Rx antennas ... ?
6. Could you please provide us with some more information about the antennas layout ? Size ? Datasheet ?