Part Number: TMP390
Tool/software:
Hi ti team,
The current problem is that the temperature fluctuates from 0 to 5 degrees, and the temperature lag function is lost. Please confirm if it is normal?
The chip was tested in a high and low temperature chamber from -5 degrees to 50 degrees. The resistance was set to low temperature 0 degrees protection, hysteresis +5 degrees recovery. I hope to see the interval of 0 to 5 degrees remain in the protection state, without any jump, and wait for the temperature to rise to 5 degrees before exiting the protection.