Other Parts Discussed in Thread: MMWAVE-L-SDK
Tool/software:
Hi,
I recently updated the MMWAVE-L-SDK from 5.5.2.0 to 5.5.3.0 and found the debug.appimage I built or from prebuilt_binaries folder can not run with visualizer. After sending the cfg (e.g. motion and presence detection), the visualizer kept showing "No data detected on COM port, read timed out". The release.appimage is fine though.
If I disable low power mode (set lowPowerCfg to 0), then debug.appimage works normally. This doesn't happen on MMWAVE-L-SDK 5.5.2.0. Both debug and release build work fine with lowPowerCfg=1.
May I know why? I understand that when using debugger with debug build we need to prevent the device going into low power mode, however, I'm not running debugger to do step-by-step debugging.
Thanks,
Laker