Tool/software:
I can run the IWR6843ISK with mmWaveStudio in software trigger or hardware trigger. When I use the default settings in mmWaveStudio, I get samples/chirp = 256, chirps = 128, and frames = 8. This amounts to the correct calculated number of words in the adc_data.bin file. when software triggered. However, when I trigger with hardware input, the number of words is 1/8 the total. I assumed this was then doing only 1 frame, but the data doesn't appear to be stored in that format. Please tell me now the hardware triggered data is stored in the file.
The way I can tell, is if I plot say chirp 1 antenna 1 frame 1 vs chirp 2 antenna 1 frame one, the data is almost an exact overlay, as expected. But using hardware trigger, the data does not match very well.
Please give me the new format. It is not in the documentation that I can find.
Regards,
Larry