Tool/software:
I’m working on a project where I need to measure a distance of 15 mm between a sensing coil and a metal target. While I’ve already ordered the LDC1614EVM evaluation board and I know it can be interfaced with an Arduino, I’d prefer not to use it as it makes the circuit bulkier. Instead, I want to design a custom PCB using the tiny LDC1614 (4 mm x 4 mm x 1 mm) chip and connect it directly to an Arduino Nano.
Is it feasible to create this compact setup with the LDC1614, or are there any challenges I should consider?
Thanks,
Ahmed