We have an application that needs a minimum absolute voltage on the DXP pins of the TMP513 due to ESD protection under some conditions. Is it OK to ground the corresponding DXN pin so that the DXP pin will only be +0.8V or so? We have tried this and the preliminary results were bad. The data sheet seems to be silent on the allowed connections. If left without an external DC path, the DXN pins go to about +0.7V and the DXP pins go to about +1.4V. This last voltage is the problem as there is then current through an ESD diode for some chip configurations.
If we can't ground the DXN pins, is there a minimum voltage (say 0.3) that would still allow the TMP513 to work properly?
Thanks,