Tool/software:
Hi,
I understand that the TxGainTampLUT has entries in 10 degree increments, such as 30 to 40 degrees, 40 to 50 degrees, etc.
Is the reference temperature used in selecting the LUT the temperature obtained by the mmwavelink API rlRfGetTemperatureReport?
rlRfGetTemperatureReport gives temperature information for Tx, RX, Pm, and Dig.
Which of these values will be used for LUT selection?
Best Regards,
Hiroyuki Taguchi