This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432AOPEVM: Assistance with Connecting IWRL6432AOPEVM and MMWAVEPOEEVM

Part Number: IWRL6432AOPEVM
Other Parts Discussed in Thread: MMWAVEPOEEVM, , MMWAVEICBOOST

Tool/software:

Dear Sir/Madam,

I am a newcomer(really a rookie) to the TI mmWave sensor field and currently have two boards: IWRL6432AOPEVM and MMWAVEPOEEVM. I would like to use the Power over Ethernet (PoE) board to power the IWRL6432AOPEVM and also transmit data to the host system(for example my PC). I want to send an example instruction to the board, then it returns the data via Ethernet.

I have followed the user guide for MMWAVEAOPEVM, but it only provides instructions for "MMWAVEICBOOST and IWRL6843ISK." Unfortunately, there is no information on how to connect the boards I have.

Since point cloud data may involve a large amount of data transfer, I am considering using SPI(I normally use I2C more often) communication between them. Could you please advise on how to connect these two boards? Additionally, is there a simple demo available for testing?

Thank you for your support.

Best regards,
Carol