This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT4060DTSEVM: interrupt singnal issue

Part Number: OPT4060DTSEVM
Other Parts Discussed in Thread: OPT4060,

Tool/software:

here is a question which i want to make sure with you,  it is a problem which is about interrupt modes. I test the OPT4060DTSEVM, and set the FAULT_COUNT is 4, the HIGH_LIMIT is 4095, and the conversion time is 300ms, when i give a high power light to opt4060 about 5s, it triggers and give the interrupt singnal....

but when i try to use a flash light, and the falsh frequency is about 1HZ,  it can not give the interrupt singnal no matter how long i give the flash ligh?  

For opt4060, how it detect the fault count?  Isn't this fault count cumulative?  if the duration of the high power time can not achive 4 fault conversion time, will OPT4060 reset the fault count ?

Does it mean i can not use the flash light to let OPT4060 give the interrupt singnal?