Other Parts Discussed in Thread: USB2ANY
Tool/software:
Hi,
We are currently unable to activate OWI at around 30-50% of our sensors using PGA305 with 4-20mA mode.
This has not always been a problem and we have had 100's of these sensors working perfectly fine, but now there is a big issue with activating OWI that was introduced just recently.
We have tried all kinds of combination of Rloop and additional voltage, nothing's working. And we have also measured the voltage and timing of OWI activation signal which seems to be correct according to datasheet, but there is no reply signal from PGA305.
This activation issue is only an issue when we have the electronics with PGA305 installed in a sensor. If we take the electronics out of the sensor, we are able to activate OWI, but not when it is installed in a sensor.
When the electronics is installed in the sensor it is connected to a wheatstone bridge of around 2.7k impedance and a temperature sensor.
The PGA305 is also programmed with calibration coefficients and scaling factors that do not correspond to the wheatstone bridge it is connected to, and the current we measure is around 3.1 mA to 3.4 mA.
We have found that if we delete the calibration coefficients and scaling factors, change Vbrg to a lower voltage or increase iTemp we are able to activate OWI.
But we have not found the root cause of why we are not able to communicate.
We have made some changes in EEPROM from the sensors that was working fine to the sensors with this issue.
See below picture for EEPROM data in sensor with issues to left and to the right is EEPROM data in sensor with no issues activating OWI: