Other Parts Discussed in Thread: MMWAVEICBOOST
Tool/software:
Hi,
Referring to the previous thread IWR6843: IWR6843 firmware update over CAN - Sensors forum - Sensors - TI E2E support forums continuing this new thread.
Summarizing all together, I am trying to update firmware of IWR6843ISK radar module over the air. I am referring TI's CAN_SBL. I am able to run the bootloader successfully but while updating the firmware or transmitting the binary file over CAN using PEAK CAN analyzer I am not able to receive anything on radar module side. I tried correcting parameters and as suggested I tried to check the interrupt bit of CAN. It is not getting any interrupt when I check for the interrupt status using MCAN_getIntrStatus(0xFF500000); this function.
Just to clarify, which CAN transceiver are you using, MCANA or MCANB? - MCANA or MCANB you mean CAN connectors? I am connecting it to the J3 connector of IWR6843ISK.
Thanks,
Manoj