Tool/software:
Hi expert,
SensorTech update their SBL from SDK 4.4.1.2 (awr294x_09_00_00_15) to SDK 4.6.1.2 (awr294x_09_02_00_15), and their application is still on SDK 4.4.1.2.
And they find Bootloader_runSelfCpu in the end of SBL is not able to jump to application sometimes. According to the function as below, it should not return from this function but we saw it returned. The issue possibility is quite low (0.1% ~ 1%).