Part Number: MMWAVE-STUDIO
Tool/software:
Hello!
When trying to execute a lua script and using a library in order to enable xml parsing (luaexpat which itself uses the expat c library) I get the following error: error loading module 'lxp' from file '.\lxp.dll':
[14:29:16] Das Betriebssystem kann %1 nicht ausführen.
The DLLs are all located in the RunTime folder of the mmWaveStudio folder under C:\ti, all DLLS were compiled for lua5.1 and for a 32 bit system as mmWaveStudio runs in 32 bit and using lua5.1. Furthermore the script works perfectly when running in a seperate environment that also uses lua5.1 and the same libraries, again all for 32 bit. All dependencies seem to be accessible to mmWaveStudio through the system Path and environment, however, I suspect that a difference in environment may be the issue. Is there a way to see environment details and compare them to the other environment that the script runs in? Maybe someone has some other recommendations for troubleshooting steps I can take. Thank you!