This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC2010: Datasheet errata

Part Number: HDC2010

Tool/software:

SNAS693D; Feb 2021 revision:

Section 7.3.1

"The DRDY/INT_EN bit (0x0E bit[2]) must be set to 1 and the INT_MOD bit should be set to 0. If these bits are not configured, the pin will be left in
high impedance"

This is not correct as the INT_MOD bit can be either 0 or 1.

Table 7-14 is incorrectly labeled.

  • Hi Mike,

    I think you are correct. I believe the table is right, but the text in the DRDY section implies it must be set to 0 to get the DRDY pin to work. Thank you for catching this, we should amend the text to clarify that the INT_MODE bit doesn't determine the DRDY status.

    Thanks

    -Alex Thompson