Tool/software:
I want try to make bike radar example which is included at radar toolbox example project.
I have some questions about this project.
1. Is the speed of the bicycle calibrated to the speed of the target?
For example the speed of the bike is about 30km/h and the target(car) speed is 40km/h.
In this case the output of the speed is 10km/h or 40km/h?
If this project does not calibrate the speed of the bike, the user shoud calibrate with the speed of the bike?
2. Can I know about the details of the demo specific cli command?
There are two specific parameter like as below. I cannot find the meaning of the items of each parameter.
Could you explain about that?
extendedMaxVelocity <enabled> <numerator> <denominator> <numHypothesis> <spreadDopIndx> <spreadRngIndx> <isDetMatrixLogScale>
dynClutterRemoval <Enabled><lambda> <xNearThr> <yNearThr> <rlsMaxInlierErr> <vClutterMaxErr> <keepClutterPoints> <resetMaxInlierErr> <inlierErrLambda> <noUpdateFrmCntrThr>