This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-DSP-EVM: ADC data file

Part Number: MMWCAS-DSP-EVM
Other Parts Discussed in Thread: MMWCAS-RF-EVM

Tool/software:

Hello,

I have the MMWCAS-RF-EVM board and the MMWCAS-DSP-EVM board, and I'm trying to set it up with the help of mmWave Studio.
I know that I can get one ADC data file with the size of the set number of frames.
Is there a way to get one ADC data file with the size of one frame for the set number of frames?
(For example, if the set number of frames is 10, I would like to know if there is a way to get 10 ADC data files with the size of one frame.)

Regards,
Tsuda

  • Hi,

    it is possible to open the original bin file in matlab or python and create 10 ADC files for each frame. The size of the frame is computed based on the chirp configuration

    It is not possible to get directly 10 ADC files.

    thank you

    Cesar