Tool/software:
Good afternoon,
I am trying to configure the IWR6843ISK radar unit to read data up to 100m. I made a custom configuration file with the mmwave sensing estimator and in MATLAB tried to configure the sensor with the example RecordProcessADCDataTIRadarBoardExample. I have it working with config files that are made for up to 25m of range but not for the one with the longer range one we made. Is this due to the prebuilt binary uploaded to the board and if so, is there a demo binary made for up to 100m of range or is there an application to make a binary that will solve this issue?
Thanks,
Nikolas