Other Parts Discussed in Thread: IWRL1432, SYSCONFIG
Tool/software:
Hai,
My team is working on a level sensing application using the IWRL1432. We obtained the source code from Resource Explorer and imported it into Code Composer Studio (CCS).
- I need to send the level sensing data via UART. I noticed that the UART driver is already enabled in the SysConfig file, so I used the
CLI_writefunction to send the data (which is present indpc.c). However, I am not receiving any data over UART. Do I need to make any hardware modifications to enable this? - I also enabled the SPI driver to send data to an external MCU. I wrote the necessary code and built it, generating a
.appimagefile in the debug folder. I assume this is the file that needs to be flashed onto the board, correct?
Current SPI Connections:
- MOSI → J9 (Pin 12)
- MISO → J9 (Pin 14)
- SCLK → J8 (Pin 13)
- CS Pin → Not required (Is this correct?)
Could you suggest the next steps I should take to proceed?