Other Parts Discussed in Thread: AWR2944, AWR2944EVM
Tool/software:
Hi everyone,
I noticed that the mmWave Sensing Estimator doesn’t include boards like the xWR2243, which has a 4Tx/4Rx antenna configuration. I’m looking to compare its performance with the xWR1843AOP, which features an Antenna-on-Package (AoP) design but has only 3Tx and 4Rx antennas.
Some key questions I have:
- Antenna Configuration: Does the additional transmitting antenna on the xWR2243 provide a significant advantage over the xWR1843AOP’s AoP design?
- Transmitted Power & Noise Figure: The AoP design of the xWR1843AOP benefits from increased transmitted power and a lower noise figure—does this compensate for having only 3 transmitting antennas instead of 4?
- Field of View & Resolution: How do these differences in antenna design affect angular resolution, field of view, and overall sensing capability?
- Other Considerations: Are there any additional factors I should keep in mind when making this comparison?
I’d appreciate any insights from those who have experience with these boards.
Thanks!