Tool/software: TICloudAgent, TICloudAgentBridge, mmWave Demo Visualizer (v3.5.0)
Hi, I have the following problems with my mmWave eval board:
Issue Description:
I'm experiencing intermittent data transmission with my IWR6843AOPEVM Rev. G radar sensor. The device is:
- Running the pre-built OOB binary for SDK 3.5
- Connected to the mmWave Demo Visualizer (v3.5.0)
- Using Google Chrome with TICloudAgentBridge Extension and latest TICloudAgent
- Configured with all SOP switches in OFF position for USB communication
The sensor consistently stops transmitting data after a brief period (1-15 seconds, typically 8-9 seconds).
Troubleshooting Steps Attempted:
I can temporarily restore functionality by:
1. Power cycling the device and reloading the configuration
2. Partially disconnecting only the USB D+/D- pins (leaving VUSB and GND connected), then reconnecting
- When doing this, the USB_LED LD4 (located next to the 40 MHz crystal) turns off
- When fully reconnected, the device resumes data transmission without reloading the configuration
In both cases, the eval board will stop transmitting after the same time periods as described above.
Additional Information:
- The device has already worked flawlessly
- Has been unused for about a month, now has the aforementioned problems
- The issue persists across multiple reboots, computers, and operating systems
Can you help identify the cause of this intermittent data transmission and suggest a permanent solution?