Other Parts Discussed in Thread: DCA1000EVM, IWR1642
Tool/software:
We have set up the IWR1642EVM and DCA1000EVM boards as described in the TCA1000EVM Quick Start Guide. The image below displays our current setup, the white cable is our USB connection to the computer and the black cable connects to our 5V power supply.
When connecting the boards to our computer via USB cable, it is not detected under "Other Devices" or "Ports(COM)" (shown below). The computer is running on Windows 11; we have attempted to add COM ports through the device manager, but it appears we don't have them.
We only can see 4 EVM ports but not 2 XDS110 ports.
We have installed proper driver but still cannot proceed.
The LED (5V led and NRST) on the IWR1642 board are blinking at the same time.
We believe that it is the problem and want to know the meaning of the blinking.