Other Parts Discussed in Thread: LDC1614-Q1
Tool/software:
Hi colleagues,
Here are a few questions about the IC performance.
A design using LDC1612-Q1/LDC1614-Q1 IC to sense a target moving. The travel distance is about 4mm, the travel direction is along the PCB board surface, the airgap between the target and the PCB surface is a constant value under ideal conditions.
After sample assembly and the sensor calibration:
1. How sensitive is the sensor to the airgap variation under vibration?
2. Is the sensing accuracy affected by unbalanced airgap?
3. Is the sensing accuracy sensitive to the ambient temperature, from -40C to +125C?
3. In a website source, https://www.ti.com/document-viewer/lit/html/SSZTCL3
a. What does the code change mean?
b. What is the y-axis presenting?
Would anyone please provide some information that can answer the questions above?
Thank you.