Other Parts Discussed in Thread: FDC2214
Tool/software:
The FDC2214 capacitance-to-digital converter is specified to reach a maximum output rate of 4.08 kSPS. However, my measurements using the evaluation module show a 2.5 ms/sample (400 SPS) readout time. The Sensing Solutions GUI is configured to the EVM output rate so that it does not limit the data collection speed. Also, changing the settle count seems to have little effect.
If I understand correctly, 40 MHz is the maximum external oscillator frequency. The GUI itself indicates a 26.625 ms Total Device Sampling Time at this clock frequency during single channel measurement. Therefore, I am quite confused about how the 4.08 kSPS output rate can be achieved. I would very much appreciate any advice!