Part Number: IWRL1432BOOST
Other Parts Discussed in Thread: IWRL1432
Tool/software:
I am currently using the IWRL1432 board for a level sensing application. After flashing the pre-built binary, I am using the default configurations. However, the maximum detection range is only 3 meters, whereas I need at least 10 meters.
To achieve this, I used the mmWave Sensing Estimator to generate configurations, but I couldn’t find specific settings for level sensing.
- Could you provide configuration settings for a 10-meter detection range or point me to a relevant source?
- In the command
channelCfg 1 1 0, I understand that it enables 1 TX and 1 RX. To increase the detection range, should I enable additional TX and RX channels? - If I enable all 3 RX and 2 TX, what will be the expected power consumption?
Thanks & Regards,
Amara Rakesh