This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243BOOST: How awr1243 is developed

Part Number: AWR1243BOOST
Other Parts Discussed in Thread: AWR1243, AWR2944, AWR1642, AWR1843

Tool/software:

Awr1243 does not have an integrated ARM or DSP core, so it does not support mmwave sdk, so it is impossible to use ccs modulation. Then there is another way to adjust or develop awr1243.

  • Hello Zhao,

    The AWR1243 is a front device only. It needs a processor paired with it function that is why it does not have a programmable core.
    This is used mainly for cascade purpose when you want multiple front end devices and a single processor to process the combined data.
    If you are looking at a soc which has programable core you can take a look at awr1843, awr1642, awr2944, etc.

    Regards,
    Saswat Kumar