This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP104: TMP104EVM Kit

Part Number: TMP104
Other Parts Discussed in Thread: TMP144EVM

Tool/software:

Hi all,

I am looking for TMP104EVM. However, I cannot find it on Ti.com and only software is listed.

TMP104EVM Evaluation Board and Software Tutorial

1) Can I order TMP104EVM currently?

2) If it is discontinued, why is it discontinued? Is there a problem with the EVM?

Best Regards,

Ryusuke

  • Hello Ryusuke,

    This EVM was discontinued due to the SM-USB-DIG module's discontinuation. Without it the EVM could no longer be used. If you are interested in a UART-compatible temperature with an EVM I would recommend the TMP144. Although it is not software-compatible with the TMP104, it has better accuracy (1C vs 2C) and temperature resolution (12-bit vs 8-bit) and is also available in a DSBGA package.

    Here is the link for the TMP144EVM too: https://www.ti.com/tool/TMP144EVM.

    Regards,

    Harry