Other Parts Discussed in Thread: MSPM0L1306, , TMAG5273, MSP432E401Y
Tool/software:
Hi Alison, this is a follow up of my request for information on the TMag3001evm mspm0l1306 evm question. here is my request again:
Hi Alison, You successfully helped me before, and I'm hoping you can again.
I have the example TMAG3001/TMAG5273 mspm0l1306 evm you sent working successfully.
I also see you have about 1700 lines of code from two years ago on TMAG5273 MSP432E401Y which I downloaded and have hardware to run. I see several additional examples I could use,
so I hope to see code details and convert them from simplelink to mspm0l1306.
However I have a problem. The examples use a different compiler than ticlang. and I get the error "No TI Arm compilers, supporting device 'MSP432E401Y', are currently installed"
I have the simplelink_msp432e4_sdk_4_20_00_12 installed.
What compiler do I need, where do I download it, and how do I install it.
Is there anything additional I need or have to do?
eric@avidasw.com edulicki@avidasw.com
Can you provide me with any update on my question? Thanks.