This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: Sensors forum

Part Number: IWR1843BOOST
Other Parts Discussed in Thread: IWR1843, AWR1243, AWR2243

Tool/software:

Hi

Similar to that of IWR1843 Do we have any tool which helps to collect point cloud data for AWR1243.

Regards 

Gopal  

  • Hi,

    Please consider AWR2243 instead of AWR1243.

    AWR2243 is a sensor only device. In order to create point cloud data one would need to 

    • use mmWave Studio and DCA1000 capture card to capture raw data.
    • write matlab or python scripts to process the data and create the point cloud.

    thank you

    Cesar

  • Hi Cesar,

    I am aware of a MATLAB script which converts .bin to .mat file which is then converted to radar cube.

    But, I am unable to find any reference which converts .bin to point cloud format which i can further use in MATLAB. 

    Regards 

    Gopal

  • Hi,

    We do not provide matlab/python code to process the raw data. You would need to develop this code yourself.

    Thank you

    Cesar