Tool/software:
Hi, I am getting the error: MSS Power Up async event was not received! evry time I try to run a Lus script or try to connect via SPI to any chip.
Could you provide some help please?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi, I am getting the error: MSS Power Up async event was not received! evry time I try to run a Lus script or try to connect via SPI to any chip.
Could you provide some help please?
Hi Javier,
What power supply are you using?
Could you provide the entire mmWave Studio log?
Thank you,
Jin
I am using a 12 V 3 A power supply. I am using mmwave-studio 03.00.00.14. Here is the log:
GM: Constructor
GM: Thu Mar 13 13:41:01 2025
RSTD.Transmit("/Settings")
[13:41:01] System.FormatException: La cadena de entrada no tiene el formato correcto.
[13:41:01] en System.Number.ParseSingle(String value, NumberStyles options, NumberFormatInfo numfmt)
[13:41:01] en RSTD.frmLuaShell.RstdGuiSettingsToLuaShellLayout()
[13:41:19]
[13:41:19] ### Running Startup script: "C:\ti\mmwave_studio_03_00_00_14\mmWaveStudio\Scripts\Startup.lua" ###
[13:41:19] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[13:41:19] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[13:41:19] Scripter ignored: Attempt to UnBuild() again or before Build.
[13:41:19] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_03_00_00_14\\mmWaveStudio\\Clients\\\\LabClient.dll")
[13:41:19] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[13:41:19] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[13:41:19] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[13:41:19] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[13:41:19] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[13:41:19] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_03_00_00_14\\mmWaveStudio\\RunTime\\SAL.dll")
[13:41:19] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[13:41:19] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[13:41:19] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[13:41:19] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[13:41:19] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[13:41:19] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[13:41:19] RSTD.Transmit("/")
[13:41:19] RSTD.SaveSettings(): Settings saved to "C:\Users\jcejudo\AppData\Roaming\RSTD\config.xml"
[13:41:19] RSTD.Build()
[13:41:19] RSTD.SaveSettings(): Settings saved to "C:\Users\jcejudo\AppData\Roaming\RSTD\config.xml"
[13:41:19] RSTD.Transmit("/")
[13:41:19] RSTD.AL_Build()
[13:41:19] RSTD.AL_LoadXml()
[13:41:19] RSTD.Transmit("/")
[13:41:19] RSTD.AL_Init()
[13:41:19] RSTD.Clients_Build()
[13:41:19] GM: Init
[13:41:19] GM: Loaded 'C:\ti\mmwave_studio_03_00_00_14\mmWaveStudio\Clients\\LabClient.dll'
[13:41:19] GM: 1 Guest (s) init
[13:41:19] GM: 1 Module(s) init
[13:41:19] GM: 2 Tab (s) init
[13:41:19] RSTD.Client_LoadXml()
[13:41:19] [RadarAPI]: ar1.selectRadarMode(0)
[13:41:19] [RadarAPI]: Status: Passed
[13:41:19] Matlab Runtime Engine is installed
[13:41:19] [RadarAPI]: Starting Matlab Engine..
[13:41:23] [RadarAPI]: Matlab Engine Started!
[13:41:24] [RadarAPI]: ar1.selectCascadeMode(0)
[13:41:24] [RadarAPI]: Status: Passed
[13:41:24] [RadarAPI]: ar1.LoadSettings('C:\Users\jcejudo\AppData\Roaming\RSTD\ar1gui.ini')
[13:41:24] [RadarAPI]: Error: Índice fuera de los límites de la matriz.
[13:41:24] Trace:
[13:41:24] en AR1xController.ScriptOps.getMatlabPostProcVersion()
[13:41:25] TESTING = false
[13:41:25] RstdNet: Port 2777: Listening..
[13:41:25]
[13:41:25] ***Script completed successfully.***
And when trying to load a script:
[13:42:05] LuaLoad("C:/ti/mmwave_studio_03_00_00_14/mmWaveStudio/Scripts/Cascade/Cascade_Configuration_MIMO.lua")
[13:42:10] Setting up Studio for Cascade started..
[13:42:10] [RadarAPI]: ar1.SelectCaptureDevice("TDA2XX")
[13:42:10] [RadarAPI]: Status: Passed
[13:42:10] [RadarAPI]: TDAStatusCallback Event Registered
[13:42:10] [RadarAPI]: registerTDAStatusCallback Status: Passed
[13:42:10] [RadarAPI]: ar1.ConnectTDA("192.168.33.180", 5001, 15)
[13:42:10] [RadarAPI]: Device 32 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0
[13:42:10] [RadarAPI]: Device 32 : CAPTURE_RESPONSE_VERSION_INFO Async event recieved() with status 0. TDA Version : REL_VISION_SDK_03_07_01_00 Aug 5 2019 15:04:45[13:42:10] [RadarAPI]: Device 32 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0
[13:42:12] [RadarAPI]: Device 1 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0
[13:42:12] [RadarAPI]: ConnectTDACaptureCard Status: Passed
[13:42:12] TDA Capture Card Status : CONNECTED!
[13:42:12] ConnectTDA Successful
[13:42:12] [RadarAPI]: ar1.selectCascadeMode(1)
[13:42:12] [RadarAPI]: Status: Passed
[13:42:12] selectCascadeMode Successful
[13:42:12] Setting up Studio for Cascade ended..
[13:42:12] [RadarAPI]: Device 1 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0
[13:42:13] [RadarAPI]: Device 1 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0
[13:42:13] [RadarAPI]: ar1.FullReset(1)
[13:42:13] [RadarAPI]: Status: Passed
[13:42:13] [RadarAPI]: ar1.SOPControl_mult(1,4)
[13:42:13] [RadarAPI]: Status: Passed
[13:42:13] Master : SOP Reset Successful
[13:42:33] [RadarAPI]: ar1.PowerOn_mult(1, 0, 1000, 0,0)
[13:42:33] Status: Failed, Error Type: RESP TIMEOUT
[13:42:37] MSS Power Up async event was not received!
Hi Javier,
Could you try with a 12V 5A power supply for the MMWCAS-DSP-EVM?
This is the typical power supply for the MMWCAS-DSP-EVM: https://www.ti.com/lit/ug/spruis6/spruis6.pdf
Thank you,
Jin
I fixed the issue. Just to let you know, in case other customer is experiencing the same problem: I just disconnected both boards, MMWCAS-RF-EVM & MMWCSA-DSP-EVM, I disconnected the SSD also and connected everything back again. Now, it works as it used to do...It seems some kind of hardware connection problem. Thanks anyway!
Hi Javier,
Glad to hear it was resolved. Thanks for sharing your solution.