This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2214EVM: Sensor design and optimization

Part Number: FDC2214EVM
Other Parts Discussed in Thread: FDC2214, FDC1004EVM, LDC1612EVM, FDC1004, LDC1312, FDC2112, FDC2212, LDC1612

Tool/software:

Hi everyone,
I'm currently working with the FDC2214EVM – High Resolution L-C Sensing Evaluation Module, and I’m looking for more detailed information about the recommended range of inductance, capacitance, and resistance for the LC sensors that can be connected to the FDC2214.

I’ve found some general specifications in the documentation:

  • Sensor Type: LC Resonant Circuit (Inductance + Capacitance)
  • Sensor Operating Frequency: 10 kHz – 10 MHz (optimal: 1–5 MHz)
  • Typical Inductance: 1 µH – 20 µH
  • Typical Capacitance: 10 pF – 330 pF
  • Recommended Quality Factor (Q): Q > 10, ideally Q > 30 for better sensitivity and stability
  • Recommended Parallel Resistance (RP): RP > 300 kΩ

Are there any official guidelines or application notes from TI (or community experience) that suggest more specific recommended or optimal ranges for L, C, and RP in different use cases or sensor configurations?
I’d also be interested to know if there are any software tools or calculators that can help with the design of LC sensors (e.g., selecting appropriate inductor/capacitor values, estimating resonant frequency, Q factor, or simulating sensor behavior).

Are there similar tools also for FDC1004EVM and LDC1612EVM?

Any suggestions, links would be greatly appreciated!
Thanks in advance!