This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: Handling backup region of SBL

Part Number: AWR2944
Other Parts Discussed in Thread: AWR2544, UNIFLASH

Tool/software:

Hi Experts,

I have a question regarding to the backup regions of SBL. As I read from AWR294x and AWR2944LC Technical Reference Manual

And the below is the statement from Application note AWR294x, AWR2x44P, AWR2544 Primary and Secondary Bootloader

So my questions are:

  1. Erase or flashing new image of SBL on backup region on external flash is user option or it should be not erased/flashed?
  2. And the offset on flash for back up region is 0x00040000. It means the size of SBL shall be 256K. Can I change this offset in case of my SBL size is larger than 256K?